Cancel
Showing results for 
Search instead for 
Did you mean: 

Student Design Contest

  • My name is Mark Keaney, I am a current Mechanical Engineering student at the University of Alabama in Huntsville, and am submitting the render for our second design project for Introduction to Computational Tools.Keaney_climber_keyshot.4.jpgRibbon Climber

     

    Using NASA's Tether and Robot Climber Contest as inspiration, I have modeled my own version of a tether climber.  Mine is a scaled down version of those submitted by the various teams for NASA's contest but uses similar design concepts. Namely, the use of multiple wheels to provide traction on either side of the tether, and the use of photovoltaic arrays to generate power. 

     

    The primary difference is that the goal of my own design work was to find ways to achieve the desired types and directions of motion using only one simulated motor in the Solid Edge program. I achieved this through a combination of carefully placed rack and pinion gears (for horizontal movement), standard gear relationships, linear motion relationships, and the physical motion option on the simulate motor tab.  

     

    The rack and pinion are used to move the driving wheel into position against the tether which then drives the tether downward through the 4 guide wheels at the top.  

     

    Video of the movement

    Robot Tether Climber

    Dreamer

    My name is Mark Keaney, I am a current Mechanical Engineering student at the University of Alabama in Huntsville, and am submitting the render for our second design project for Introduction to Computational Tools.Keaney_climber_keyshot.4.jpgRibbon Climber

     

    Using NASA's Tether and Robot Climber Contest as inspiration, I have modeled my own version of a tether climber.  Mine is a scaled down version of those submitted by the various teams for NASA's contest but uses similar design concepts. Namely, the use of multiple wheels to provide traction on either side of the tether, and the use of photovoltaic arrays to generate power. 

     

    The primary difference is that the goal of my own design work was to find ways to achieve the desired types and directions of motion using only one simulated motor in the Solid Edge program. I achieved this through a combination of carefully placed rack and pinion gears (for horizontal movement), standard gear relationships, linear motion relationships, and the physical motion option on the simulate motor tab.  

     

    The rack and pinion are used to move the driving wheel into position against the tether which then drives the tether downward through the 4 guide wheels at the top.  

     

    Video of the movement

  • Here is a render of my class project, a bridgeport mill 

    bridgeport mill

    Dreamer

    Here is a render of my class project, a bridgeport mill 

  • My entry is of my high tech windmill.  I made the body of the windmill clear to show the working components of the motor.  My windmill is not like your old school windmills it is new and improved with different materials and colors.  I attend University of Alabama in Huntsville.  Gann_Renderedimage.jpg

    Newly Updated Windmill

    Dreamer

    My entry is of my high tech windmill.  I made the body of the windmill clear to show the working components of the motor.  My windmill is not like your old school windmills it is new and improved with different materials and colors.  I attend University of Alabama in Huntsville.  Gann_Renderedimage.jpg

  • My name is Csaba Juhasz. I made a multifunctional printer. I designed by Solid Edge. I rendered the picture with Keyshot. I am from Hungary. I study in Kecskemet, Hungary at Pallasz Athene University as mechanical engineer. 

    Multifunction printer

    Theorist

    My name is Csaba Juhasz. I made a multifunctional printer. I designed by Solid Edge. I rendered the picture with Keyshot. I am from Hungary. I study in Kecskemet, Hungary at Pallasz Athene University as mechanical engineer. 

  • untitled.83.jpgMY FIRST ......PROJECT

    my self vinay kr..............

    currently i am persuing diploma from "CRRIT KANJHAWALA" from mechanical stream

    i have made this design completely from "solid edge st 8"...the assembly of 495 parts was also done from "solid edge st8" ....and the rendering was done via "keyshot render"

    it tooks of about 28 days hard work to complete it,,,,,......

    this design is one of the greatest achievement .......according to me.....

    This is the render image of my engine project....this is a petrol engine comprises with 7 pistons....generating a power of about 1900 cc...........which comprises with my new innovative technology.....which i named as "the electronic valve technology".....this replaces the old arrangement of camshaft and timing chain and a lot of mechanical parts with a small component which i named as solenoid valve....these valves are electricity operated which run on 12 volts dc current......there are two types of valve one is inlet solenoid valve (which is connected to the inlet port of engine...and comprises with injector in it to inject fuel) and the other is exhaust solenoid (which is connected to the exhaust manifold).......my design can be illustrated completely by the attachements given below.....

    thanks to siemens for giving me a platform on which i may show my self that what i am.....

    thanks........untitled.79.jpguntitled.81.jpguntitled.80.jpguntitled.81.jpguntitled.80.jpg

    A 7 piston....generator engine.....(PETROL ENGINE IN LINE TYPE)

    Dreamer

    untitled.83.jpgMY FIRST ......PROJECT

    my self vinay kr..............

    currently i am persuing diploma from "CRRIT KANJHAWALA" from mechanical stream

    i have made this design completely from "solid edge st 8"...the assembly of 495 parts was also done from "solid edge st8" ....and the rendering was done via "keyshot render"

    it tooks of about 28 days hard work to complete it,,,,,......

    this design is one of the greatest achievement .......according to me.....

    This is the render image of my engine project....this is a petrol engine comprises with 7 pistons....generating a power of about 1900 cc...........which comprises with my new innovative technology.....which i named as "the electronic valve technology".....this replaces the old arrangement of camshaft and timing chain and a lot of mechanical parts with a small component which i named as solenoid valve....these valves are electricity operated which run on 12 volts dc current......there are two types of valve one is inlet solenoid valve (which is connected to the inlet port of engine...and comprises with injector in it to inject fuel) and the other is exhaust solenoid (which is connected to the exhaust manifold).......my design can be illustrated completely by the attachements given below.....

    thanks to siemens for giving me a platform on which i may show my self that what i am.....

    thanks........untitled.79.jpguntitled.81.jpguntitled.80.jpguntitled.81.jpguntitled.80.jpg

  • CLAAS 980 (type 497) forage harvester

    The challenge was to select a product to evaluate ergonomically. Given that I had a background in agriculture, I chose a Jaguar Claas 980 - specifically the type 497 as this was a new prototype model set for release in 2017. The product was modelled and rendered in Siemens NX 10, then transferred to SAMMIE for ergonomic evaluation, alongisde final rendering in Adobe Photoshop.

     

    About me

    I'm currently in my second year of studynig Product Design Engineering (MEng) at Loughborough University.

    Top of the CLAAS

    Enthusiast

    CLAAS 980 (type 497) forage harvester

    The challenge was to select a product to evaluate ergonomically. Given that I had a background in agriculture, I chose a Jaguar Claas 980 - specifically the type 497 as this was a new prototype model set for release in 2017. The product was modelled and rendered in Siemens NX 10, then transferred to SAMMIE for ergonomic evaluation, alongisde final rendering in Adobe Photoshop.

     

    About me

    I'm currently in my second year of studynig Product Design Engineering (MEng) at Loughborough University.

  • CAD Project

    Dreamer
  • Hydro Power

    Dreamer
  • Ferris Wheel

    Dreamer
  • Predator Drone

    Dreamer
  • This Grandfather Clock was created within the last five weeks as part of a MAE 211-04 class project. 

    Grandfather Clock by Madison C. Bowersox (UAH)

    Enthusiast

    This Grandfather Clock was created within the last five weeks as part of a MAE 211-04 class project. 

  • My name is Brian Austin. I am studying Mechanical Engineering at the University of Alabama in Huntsville. For my final project in my CAD class I made a watch. Here is the rendered image below.

    Watch Render.jpg

     

     

     

    Men's Watch

    Dreamer

    My name is Brian Austin. I am studying Mechanical Engineering at the University of Alabama in Huntsville. For my final project in my CAD class I made a watch. Here is the rendered image below.

    Watch Render.jpg

     

     

     

  • I made this biplane for my final Project in MAE 211 at the University of Alabama in Huntsville. 

    WACO Biplane

    Dreamer

    I made this biplane for my final Project in MAE 211 at the University of Alabama in Huntsville. 

  • Wind Turbine

    Dreamer
  • Fishing reel

    Dreamer
  • 122 total parts, 53 unique parts, and 72 moving parts.

    Twin Horizontal Steam Engine

    Dreamer

    122 total parts, 53 unique parts, and 72 moving parts.

  • This is a Keyshot render of a pitching machine that was created in SolidEdge. It has 25 unique parts and over 5 differernt working motors. When simulated, the machine will even pitch the baseball!

    Pitching Machine

    Dreamer

    This is a Keyshot render of a pitching machine that was created in SolidEdge. It has 25 unique parts and over 5 differernt working motors. When simulated, the machine will even pitch the baseball!

  • This project done in a class at the University of Alabama in Huntsville is a self designed desk fan with moving gears, and a clip for a base. It has a lighbulb on the front of the top clip, and a number of spinning objects in relation with the one motor. 

    Desk Fan

    Dreamer

    This project done in a class at the University of Alabama in Huntsville is a self designed desk fan with moving gears, and a clip for a base. It has a lighbulb on the front of the top clip, and a number of spinning objects in relation with the one motor. 

  • I created this in my CAD class at the University of Alabama at Huntsville.

    Motorcycle - Nick Brown

    Dreamer

    I created this in my CAD class at the University of Alabama at Huntsville.

  • I designed this for my CAD class at UAH (University of Alabama in Huntsville MAE 211-04)

    Walker_Floor_Fan_Render.jpg

     

     

     

    Floor Fan

    Dreamer

    I designed this for my CAD class at UAH (University of Alabama in Huntsville MAE 211-04)

    Walker_Floor_Fan_Render.jpg