Cancel
Showing results for 
Search instead for 
Did you mean: 

AMESim Crashing when using aircraft fuel system library

Experimenter
Experimenter

Hi

 

I'm using AMESim with the Aircraft Fuel System library to model a simple a/c fuel system

 

Any other example that i've tried simulating so far, using other libraries has ran fine. But when I try to run a simulation using models from the a/c fuel system library, the simulation crashes and I get the error "STDSIMDaemon.exe has stopped working"

 

Any ideas as to what might be causing this? 

3 REPLIES

Re: AMESim Crashing when using aircraft fuel system library

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hi Jethro68,

 

could you please let me know what is the release of LMS Imagine.Lab Amesim you are using and the compiler you are using as well?

 

You may find the release in the menu bar Help and then About. For the compiler settings, please select Tools in the menubar, Options, and Preferences, select the Compilation tab in the Preferences window.

 

Kind regards,

Olivier

Re: AMESim Crashing when using aircraft fuel system library

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Hi,

 

maybe you should try to recompile your system and than run the simulation.

 

Have you made any change to the sketch?

 

 

Re: AMESim Crashing when using aircraft fuel system library

Experimenter
Experimenter

Hi all

 

Sorry for the late reply

 

I did manage to solve this. Just in case anyone runs into this kind of problem, the issue was that I hadn't set the fuel definition. This caused the simulation to crash without any warnings

 

Thanks to everyone who helped me with this