Cancel
Showing results for 
Search instead for 
Did you mean: 

How to find the differences between 2 versions of a circuit

Community Manager Community Manager
Community Manager

Hi all !

 

Quick question here, if somebody can help me out.

I have two versions of the same circuit, how do I find out about the differences between them?

 

Thank you, have a nice day !

J.

6 REPLIES

Re: How to find the differences between 2 versions of a circuit

Genius
Genius
Hello Julie,
You need to load both files. Both circuits have to be in parameter mode.
Then go to Tools/Compare Systems
That's it

Re: How to find the differences between 2 versions of a circuit

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

Thanks mAx you beat me to it. All I have to do is add some pictures:

Tools/Compare systems...

 

The setup before launching the comparison:

Compare systems setup

 

And finally the outcome, you'll see the differences for:

- parameters

- global parameters

- components added/deleted

- if the connections have changed

 

Comparison results

 

 

 

 

Re: How to find the differences between 2 versions of a circuit

Siemens Phenom Siemens Phenom
Siemens Phenom

And you can copy selected parameters values from one model to the other:

 

Compare copy parameters

Re: How to find the differences between 2 versions of a circuit

Community Manager Community Manager
Community Manager

Thank you Max and Emanuel, that's very clear !!!!

Re: How to find the differences between 2 versions of a circuit

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

And if you happen to be using LMS Sysdm then you can start a compare directly from LMS Sysdm by just configuring LMS Amesim as your "diff" tool. With this you can make comparisons between several versions of your Amesim model

 

See the screenshots for more information

 

2015-06-26 12_02_49-Clipboard.png

 

2015-06-26 12_05_51-Clipboard.png

2015-06-26 12_30_11-Clipboard.png

 

Regards

Dennis

Re: How to find the differences between 2 versions of a circuit

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Colors are used to identify how models and components are different. Differences can be related to submodels, parameter values, added components...

 

colors.PNG

Patrice MONTALAND