Cancel
Showing results for 
Search instead for 
Did you mean: 

Load Global parameter

Gears Genius Gears Genius
Gears Genius

hello,

I am handling a "generic" valve  full piloted with GP.

I can switch from diverse caliber from valve with the help of GP.

For that I can load an .gp file which set the parameter for the desired caliber.

 

2 questions:

*is it possible to load the gp file with command line, or do we just have the possibilty to load it from gp window?

 

*in my gp files, I have a group a parameter "piston catalog"; unfortunately I don't achieve to reach what I want.

For instance for caliber A I have 3 pistons A1 / A2 / A3

For caliber B I have 4 pistons B1 / B2 / B3 / B4

 

when I open the gp window, I load the gp file, and I overwrite all the parameters.

Then my catalog has A1/A2/A3/B1/B2/B3/B4

 

I was expecting, that the load of gp file, loads only the pistons of the desired caliber (and not add to the present catalog)

 

I hope you understand what I mean Smiley Wink

 

thank you in advance

mAx

2 REPLIES

Re: Load Global parameter

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @mAx

 

There is no direct way to load/save gp from the command line but it's quite stratightforward to write a Python script and then use "AMEPython script.py" as a DOS command line to execute that script.

 

WIth the API in Python you will be able to :

- add gp

- remove them

- change the values of existing ones

- manage groups

 

Check in Amehelp the Function Index and search for "global" to see what's possible.

amesim_api_reference.jpg

Re: Load Global parameter

Gears Genius Gears Genius
Gears Genius

Thanks for the reply @Emmanuel_D

I think I have an issue with Python: I am unable to load a python script from cmd

I will bring it to support Smiley Wink