Cancel
Showing results for 
Search instead for 
Did you mean: 

Steam Boiler with twin horizontal cylinders

Experimenter
Experimenter

Hello,

Out of curosity, I'd like to know how to model a steam boiler with two horizontal cylinders?  I'd like to create a model with multipule flues and eventually super heating the steam.  All I need as an example of a simple model.  Thanks.

1 REPLY

Re: Steam Boiler with twin horizontal cylinders

Siemens Creator Siemens Creator
Siemens Creator

Hi Allegheny,

I recommend you to start from the physical concept (thermodynamic cycle ideally) using half heat exchanger and functional components from the TPF library. As an example, there is a very nice demo on heat pump modeling available since rev15 available here.

After that you can replace the half heat exchanger by a more detailled approach.

Keep me informed if you face any issue on this modeling.