Cancel
Showing results for 
Search instead for 
Did you mean: 

Tractor tire model

Creator
Creator

Hi,

I have to analyze the braking performance of a tractor using the Pacejka tire model. I have only the vertical load and the vertical stiffness. How can I define all the other parameters of the Pacejka formula?

2 REPLIES

Re: Tractor tire model

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Dear Barile,

 

If you have access the shape of the curve "Fx vs longitudinal slip" then you can use the tool which is linked with the tire model of the Transmission library. This is an App that you can launch from the contextual view in parameter mode in order to identify the Pacejka coefficients.

Otherwise, you can use a more simple model of tire (tanh or simplified Pacejka) and estimate the parameters.

 

Hope this will help you.

Best regards

Clem

Re: Tractor tire model

Creator
Creator
thank you clem for your reply,
I know that App but I'm trying to find the Pacejka parameters of tractor tires