Cancel
Showing results for 
Search instead for 
Did you mean: 

Step-by-step optimize your cooling system to improve a Formula Student Car performance

Siemens Enthusiast Siemens Enthusiast
Siemens Enthusiast

Founded in 1979 by the Society of Automotive Engineers (SAE) the Formula Student is an international engineering design competition for students. In only one year, students found a team, develop and build their race car to compete. This unique opportunity offers students to turn theoretical knowledge into a concrete practice. The growing popularity of the competition is proven by the fast rising number of teams and sponsors, such as Siemens PLM.

Today, the goal for Siemens PLM is to help students building more efficient, lightweight and reliable race cars from one year to the other. Modeling and simulate a race car cooling circuit  using a system approach with LMS Imagine.Lab Amesim is a way to achieve their performance target.

This step by step demo is aimed at students who want to design a more efficient cooling system for their team race car.

Description

Most teams consider the cooling circuit as an important part of the car but don’t really know about the real cooling demands of their race car. A simple cooling system in a race car consists of four components – heat sink, heart source, pump and catch can. Here, these parts are modeled in a way allowing an easy adaptation and change of the parameters.

2.png

Heat Source:

The heat is generated either by the IC-Engine or the electrical drive. To model the heating behavior a thermal capacitance from the thermal library is used. With the material icon a typical material, e.g. iron, and its thermal properties can be associated. The thermal capacity is connected to heat flow input in Watt.

3.png

Pump:

In LMS Imagine.Lab Amesim an ideal fixed displacement thermal-hydraulic pump from the thermal hydraulic library is used. Flow losses or mechanical losses are neglected. The pump is directly connected to a constant speed prime mover. Sensors before and after the pump are used to analyze the temperatures.

4.png

 

Catch Can:

The catch can is represented by a model of thermal-hydraulic accumulator, which is composed of a liquid phase and a gas phase in pressure equilibrium. To connect the catch can to the rest of the system an orifice is used.

5.png

Heat sink:

The heat sink represents the cooling component in the systemSimilar to the heat source, specific material and geometrical propertied, e.g. weight, can be associated. In order to take in account the geometry of the radiator, a thermo-hydraulic pipe with heat exchange is used. The geometrical characteristic of the radiators, e.g. diameter and length of the pipes are input data.  Additionally, the coolant properties can be set using the fluid data component located in the sketch.

7.png

 

 6.png

 

Input calculation:

The pipes of the radiator are cooled using the ambient air. The users can either set directly the mass flow of the air or the velocity of the car. The calculation is done automatically within LMS Amesim. The air properties are defined using the pneumatic gas data icon placed in the sketch.

8.png

 

9.png

 

Creation of the cooling system:

To realize a complete cooling circuit, all the subsystems described above need to be connected together in order to get following system:

10.png

Parameterization:

To find out the cooling demands of their racecar the teams only need the basic data given in the datasheets. To easily parametrize the model a user interface, called “App”, has been created using the Python capabilities of LMS Amesim. The teams can easily adjust the parameters to see how the cooling demands change e.g. when the temperature is higher or the diameter of the cooling hoses change.

 

11.png

The teams can simulate the different cooling demands for each race and make the cooling system more reliable by knowing how the different ambient temperatures effect their cooling.

 

Simulation Results 

12.pngSimulation run with 40°C ambient temperature.

 

 

13.pngSimulation run with 20°C ambient temperature.

Do you want to deploy LMS Imagine.Lab Amesim or other Siemens PLM Software tools in your team?

NB: the model will be provided to Siemens sponsored teams in order to encourage other teams to request such a sponsoring

Comments
Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Thank you Carolin for this article. That provides a good example about how LMS Amesim can help Formula Student teams to improve the design of their car. With a simple thermal model, they will be able to better size their components, optimizing the volumes and the weights, improving the performances and the reliability.

On top of that, there are also plenty of other applications where LMS Amesim could be helpful for the Formula Student teams: vehicle dynamics, engine design, powertrain electrification, transmissions, vehicle dynamics...

Siemens Creator Siemens Creator
Siemens Creator

Nice job! 

Dreamer
Dreamer

I am having trouble getting to this program after I downloaded LMS Imagine. Can anyone point me in the right direction? Thanks

Dreamer
Dreamer

Hi!

 

I am responsible for the cooling sytem for this years Lund Formula Student car. We are interested in using LMS Amesim to develop our cooling system but we don't have access to a Acadedmic bundle. This means we don't have access to the full libraby we need to create a model. Please contact me by writing a message and we could discuss this further.