Cancel
Showing results for 
Search instead for 
Did you mean: 

[Tips & tricks] – How to configure Simcenter Amesim and Simulink to launch simulation with interfaces

Community Manager Community Manager
Community Manager

You want to couple your Simcenter Amesim plant model with a Simulink control system model?

Then, you need to configure both software to enable simulation with interfaces.

Before going further ensure that you already have:

  • A license that enables to use Simulink interfaces for Simcenter Amesim
  • A license of Matlab, a Simulink software
  • An ANSI C compiler that is supported by Simulink if you are using Linux.
  • Or Microsoft Visual C++ if you are using Windows (click here to see the dedicated video)

Watch this 3-minute video to get the right method

 

(view in My Videos)

Comments
Enthusiast
Enthusiast

Hi, there I found this error while compiling the model - 

 

D:\Program Files\LMS\LMS Imagine.Lab\v1500\Amesim\AMEcompile.bat initiates a 64 bit compilation

 

Error in script usage. The correct usage is:

"C:\Program Files (x86)\Microsoft Visual Studio 14.0\VC\\bin\amd64\vcvars64.bat"

 

or

"C:\Program Files (x86)\Microsoft Visual Studio 14.0\VC\\bin\amd64\vcvars64.bat" store

or

"C:\Program Files (x86)\Microsoft Visual Studio 14.0\VC\\bin\amd64\vcvars64.bat" 10.0.10240.0

or

"C:\Program Files (x86)\Microsoft Visual Studio 14.0\VC\\bin\amd64\vcvars64.bat" store 10.0.10240.0

 

'nmake' is not recognized as an internal or external command,

operable program or batch file.

 

System build error!

 

Please somebody help me on this

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hello,

 

The current version of LMS Amesim does not support Visual Studio 14.0. Only the version up to Visual Studio 12.0 is supported. You can either install a former version of Visual Studio or install Microsoft Windows SDK 7.1. You can find the instructions to install SDK 7.1 in the link below:

 

https://community.plm.automation.siemens.com/t5/tkb/articleprintpage/tkb-id/Simcenter_1D_tkb/article...

 

Best regards,

Dreamer
Dreamer

Hello,

Actually I'm facing the above error while compiling the AMESim with Interface Block(Simulink).

 

C:\Program Files (x86)\LMS\LMS Imagine.Lab\v1510\Amesim\AMEcompile.bat initiates a 64 bit compilation

 

ERROR: The system was unable to find the specified registry key or value.

 

ERROR: The system was unable to find the specified registry key or value.

 

The x64 compilers are not currently installed.

Please go to Add/Remove Programs to update your installation.

 

Setting SDK environment relative to C:\Program Files\Microsoft SDKs\Windows\v7.1\.

 

Targeting Windows 7 x64 Debug

 Simulation Error.png

'nmake' is not recognized as an internal or external command,

operable program or batch file.

 

\LMS\LMS was unexpected at this time.

 

Please help me.

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hello,

 

Given the error message, it looks like the compilers are not correctly installed. You can try to uninstall and reinstall them by following the steps in the article in this link.

 

If you still have some issue, the best would be to contact the support by creating a request on www.siemens.com/gtac or contact by phone the local support (link here for phone number).

 

Best regards,

Experimenter
Experimenter

Hello,

 

Can we have another  video following this video?

I would like to see the whole process of the simulink to Amesim interface sir.

 

Best regards,