Highlighted

Legend Font Size of Chart

Genius
Genius

Hello,

Because some colleagues still complain about font size from my charts, I wonder if it is possible to set the font size of the legends once for all.

I don't find anything in the options.

Of course I can set the font size in the graphic, but I want it to be done automatically

Thanks in advance

Maxime

2 REPLIES 2

Re: Legend Font Size of Chart

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Hi @mAx,

 

do you mean as a default value so that all your plots always use the same fonts?

 

I think what you are looking for is called Styles in Simcenter Amesim.

 

Follow these instructions:

1. create your plot 

2. Add text and configure to the fonts you want

3. Save Style (you can make it as current directly in this window or,

 

 2018-08-24 12_08_11-Clipboard.png

4. make sure your Style is selected as "Current Style"  in the Preferences section for Post Processing

2018-08-24 12_11_25-Simcenter Amesim - [unnamed_system _].png

 

Hope this helps

 

Regards

Dennis

Re: Legend Font Size of Chart

Genius
Genius

Hello @MMMDennis

This is exactly what I was looking for

Plus, I can define "my Style" as default in options/postprocessing

Thank you!

Maxime