Highlighted

Running multiple simulations using an external script

Creator
Creator

Hi,

I am looking to run two models in such a way that I can export the results of model#1 to an external program (say Matlab), do some processing on model#1's outputs, and then use the outputs of my Matlab script to define parameter values and run model#2.

In other words, is there a way to run models from an external script?

 

What is the best way to implement this?

 

Thanks!

2 REPLIES 2

Re: Running multiple simulations using an external script

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @ameswimmer,

 

There are a couple of places you should start looking in Amehelp - F1 from Amesim:

- the demos for scripting which you can open and run

- the manual for scripting which will have some tutorials and description of all the scripts you will need

 

scripting_Amesim.png

Re: Running multiple simulations using an external script

Creator
Creator

Looks like it contains all the info I am looking for. Thank you very much!