Highlighted

ame_lic_init failed

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Dear all,

      When I used the traning license for Amesim 2019.1, The software started successfully,but when running a demo,

it said:"ame_lic_init failed:The licnesing subsystem in not initialized.Please check that the LMSLicnesDll can be found

Initialization failed"

Could someone tell me how to solved this issue?

QQ截图20190813222947.png

 

1 REPLY 1

Re: ame_lic_init failed

Siemens Phenom Siemens Phenom
Siemens Phenom
Hello, check that your environment variables are set properly. This should be done automatically during installation of Amesim. You need an environment variable %AME% which points to the installation directory and PATH should also include %AME%\win64 (where that 'missing' dll should be) but also %AME%, %AME%\win32...
If that is not the case, please reinstall Amesim with Administrator rights. If that still fails please get in touch with the person who gave you the training license.