multiple signal

Creator
Creator

Hi,
how is it here possible to multiple the signal? 23.png

Thank you
Dimo

1 REPLY 1
Highlighted

Re: multiple signal

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

no not in this way.

 

The radiation block expects one temperature on each side.

image.png

The 6 thermal masses will compute 6 different temperatures.

 

 

Either you build a distinct radation with each thermal mass or you "join the 6 masses together" to only consider one temperature.

 

For example using the 4 or 3-ports nodes (all the heat fluxes from each radiative exchange will be added together):

image.png

 

Or keeping one global radiation and connecting the N thermal masses together so that they all exchange heat with another thermal mass (using condution here):

image.png