Cancel
Showing results for 
Search instead for 
Did you mean: 

Watch the newest tech tips videos about NX CAM software

Community Manager Community Manager
Community Manager

Are you curious about what’s new in the latest version of NX CAM (January 2019)?   Watch the series of “tech tip” videos to learn how the capabilities will help you gain productivity and improve part quality.   

 

Read about all the new capabilities in NX for manufacturing here.

 

Let us know what you think of the new capabilities in the Comment section below.

 

CAM Ribbon

The CAM Ribbon is simplified, with larger pictures used for important functionality.

 

Pick on Path with IPW

In the simple Play mode, Pick on Path now displays the current status of the IPW.

 

Tool paths may now be investigated layer by layer for Operation types that cut by level.

 

Color By Motion Output Type

The Motion Output Type option is now available in the Ribbon Bar.

 

Collison Report for Guiding Curves

Variable Guiding Curves operations now detect and analyze gouges.

 

Bottom-up Cutting in Adaptive Milling

In Adaptive Milling, Bottom Up Cutting now controls stock removal between cut levels.

 

Cycles with References Generic Motion

Easily create cycle-based Generic Motion operations that can be templatized for reuse.

 

Turning Tool Holder Enhancements

Multiple enhancements allow further definition of holders for standard turning tools.

 

Gouge Check and IPW for Multi Tools

NX now supports material removal, collision check, and gouge check for multi-tools during Machine Code Based machine tool simulation.

 

Custom Feeds and Speeds

Custom Feed and Speed parameters for closed area engages can now be specicied in Cavity Mill, Rest Milling, Corner Rough, Floor and Wall, and Planar Mill operations.

 

Merge Tool Paths

Multiple operations can now be combined into a single operation containing a single merged tool path.

 

Coolant for Open and Closed Areas

Coolant options can now be specified separately for Open and Closed Areas in Planar, Cavity, Floor and Wall, and Adaptive Mill Operations.

 

Highlight Collisions in Machine Code Based Simulation

When performing Machine Code Based Simulation, collisions and gouges now highlight when you stop the simulation and drag the machine tool axis sliders or type in values.

 

Tube Milling Enhancements

Tube Roughing and Tube Finishing operations can now create the central curve automatically based on the specified Cut Area.

 

Customize Cut Level Items into Dialogs

New customizable Cut Levels items are now available for Cavity Mill, Zlevel Mill, Variable Axis Zlevel Mill, and Plunge Mill operation dialog boxes that allows you to flatten the dialog box structure.