05-09-2018 02:17 AM
Hello Team,
I'm trying to install 2 Corporate servers for same environment while installing second i am getting some issue,
Steps i have followed,
1) I have database server & instance on M/C XXXXC
2) TC_DATA & Volume for both the server should be on M/C XXXXD
2) I have installed first Corporate Server, Server Manager & Web Tier on M/C XXXXA by selecting option
"Populate database and create new data directory"
3) Now while installing second corporate server on XXXXB, i have already database which is populated & data directory on XXXXD also exists, so i have selected option
"Use populated database and existing data directory"
4) But the installation failed and gave the message like below
Executing [cd /D "D:\splmlocal\int02\appl\tc112\logs"]
Output from command: cd /D "D:\splmlocal\int02\appl\tc112\logs"
command_exit=0
Exit Status 0, elapsed time 0:00:00
...Done
Executing [preferences_manager -u=infodba -p=***** -g=dba -mode=import -scope=SITE -preference=Mail_server_charset -values="windows-1252" -action=OVERRIDE]
Output from command: preferences_manager -u=infodba -p=***** -g=dba -mode=import -scope=SITE -preference=Mail_server_charset -values="windows-1252" -action=OVERRIDE
Command line login fail! Error code = 515209 (POM_rdbms_error)
The following error has been encountered: 515209 - The operation failed due to an unexpected Database Management System error.
The report file is located at "D:\splmlocal\int02\appl\tc112\logs\1805090745\preferences_manager_20185974731.log".
command_exit=1
05-09-2018 10:01 AM
M/C XXXXC > Database Instance
M/C XXXXD > TC_DATA, Volumes
M/C XXXXA > TC_ROOT, Server Manager (PoolA)
M/C XXXXB > TC_ROOT, Server Manager (PoolB)
M/C XXXXE > TC_ROOT(.Net only), Web Tier
The mistake is selection foundation instead of just selecting server manager. I would install foundation on D where TC_DATA lives. All template deployments or additions would happen on D from then on. Select only the server manager feature when installing A/B. Also, you'll likely want to move the Web Tier to its own server (see attached diagram).
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4
05-09-2018 11:37 PM
@RandyEllsworth Thanks for the response,
But the main purpose of doing this is to have load balancing of the server,
The requirement is to have two corporate servers, don't know why they need it
M/C A --> Corporate server, .Net Server Manager, .Net Web Tier,FSC
M/C B --> Corporate server, .Net Server Manager, .Net Web Tier,FSC
Where M/C A & M/C B should have same port numbers for these services only hostname is different.
M/C D --> Should have TC_DATA & Volume for these both M/C's, Volume server is installed here with FSC.
I think it should be possible because they already have it for dev environment but I need configure it for int environment.
05-10-2018 08:39 AM
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4
05-10-2018 10:32 AM
I will collect all the data why this is necessary, and may be will come with reason.
I agree with you and the diagram which you have provided in the same way i have configured till date.
The reason they want one TC_DATA directory for both installation because they are using same database instance,
if they use different data directory as well as database instance, then we can not call it as one environment it will become two different environments.
and i dont think TC_ROOT has any entries for deployments except BMIDE projects? so no question of sync?
regarding FSC, they will be having FMS Master only on A, and not on B (but both will have FSC ).
The diagram you shared is the load balancin using multiple Server Manager by having only one Corporate Server.
and what they proposing is load balancing using multiple Corporate Server.
I will check all the details and will share as well
Thanks!
05-10-2018 11:14 AM
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4