Cancel
Showing results for 
Search instead for 
Did you mean: 

2 tier client install after enabled Active workspace

Legend
Legend

Hi

 

I have activated Active Workspace 3.1.2 in our system and today I wanted to install a 2 tier client.

During the tem setup it requiere me to add some addons like SolidWorks integration, Issue Management etc.

All of them I have a template for or are in the Tem Featueres list to select.

... but when it comes to Active Workspace I don't have that.

 

Can't find any template in the AW setup or find in the documentation how it shall be managed.

How shall I to get the Active Workspace features in my TEM setup?

 

 

Jörgen Mähler, PLM Lead Hydro
TC11.5 | TcIC11.5 | Swim 11.4 | Supplier Collaboration
NX 11,12 | Catia V5 | Solidworks 2018 | AutoCad2018
1 REPLY

Re: 2 tier client install after enabled Active workspace

Legend
Legend

... as always sometimes it's good to write to get your mind in place.

 

What I did was to reuse an old production server were I had uninstalled the configuration.

Here I didn't got the possibillity to add file locations.

 

So when I launched TEM from the 10.1.6 patch I could add the Active workspace location and it now shows up nicely in the Featueres list.

 

My mistake, sorry!

 

Jörgen Mähler, PLM Lead Hydro
TC11.5 | TcIC11.5 | Swim 11.4 | Supplier Collaboration
NX 11,12 | Catia V5 | Solidworks 2018 | AutoCad2018