Cancel
Showing results for 
Search instead for 
Did you mean: 

41178: FSC proxy error: "-9009 NO_ROUTE_3 BMIDE template installation error

Builder
Builder

Hello Team,

 

we are trying to install Customised BMIDE template in Teamcenter12 through tem.bat file 

we arre getting error like.

 

Downloading File: model.xml
41178: FSC proxy error: "-9009 NO_ROUTE_3{-1844652216}{volume/logvolume}{00e45d47f53a920cd748}".
Error updating the TC_DATA_MODEL with templates from datasets
Script execution failed.

Above error please help us to understand where its failing and how to fix it.

 

Regards

sameer kulkarni

1 REPLY 1

Re: 41178: FSC proxy error: "-9009 NO_ROUTE_3 BMIDE template installation error

Genius
Genius

Hi Sameer,

 

From the error the FSC is not able to download the model.xml from model dataset. Either the volume is not accessible(offline/Access issue) or dataset doesnt hold a named reference for corresponding model.xml dataset.

 

I prefer to check the following.

 

1. Check FSC service is up and running or not.

2. Login with infodba and try to create a dataset(any type), upload and download a reference file

3. Launch TC and check model.xml dataset and check for the named reference size and if available try to download the same.

4. If dataset reference is missing, upload the same file from %TC_DATA%\model\model.xml.

 

With these steps you should be able to pass the step.

 

Thanks

Phani