Cancel
Showing results for 
Search instead for 
Did you mean: 

AWC4.1: Content Tab doesn't work

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Good morning,

After patching from AWC4.0 to 4.1 i've this problem: when i try to show a content tab i received this error: "500 Internal Server Error".

I've installed the feature by TEM, added the "activeworkspacebom in the BMIDE, update the global constanst.image.png

 

 

 

 

 

 

 

 

 

 

 

 

 

Can you help me?

 

Thank you very much,

have a nice day.

 

Francesco

2 REPLIES 2

Re: AWC4.1: Content Tab doesn't work

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi Francesco ,

Before updating the AWC is it works properly ?

After the changes , did you put the current war file to related location ? and also did you check it with the different webbrowser?

 

Best Regards

Gurkan

Re: AWC4.1: Content Tab doesn't work

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi Gurkan,

Before updating the AWC worked properly.
I've tried to update the "activeworkspacebom" feature by Update Database Full but it was not working yet.
I've rerun the deploy of the full package of "AWC 4.1" and after the deploy the Content Tab work fine.image.png

 

 

 

 

 

 

 

I hope this solution can be useful.

 

 

Thank you very much,

have a nice day.

 

Francesco