Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Access Manager: Is there a Rule "Has No Status" e.g. "Has Status (None)"

Creator
Creator

Dear community,

 

in the Ruletree of Access Manager I can add a rule Has Status() for objects with a status of any kind or the rule

Has Status (Approved) for objects of status Approved.

 

But I wonder if there is a rule for objects with no status, e.g. Has Status (None) ?

 

I need to set ACLs for Objects in a specific project but only for objects without status.

 

In Project (ProjectXY)

  • Has Status (None) --> My ACL

Maybe someone has an idea. All suggestions are appreciated.

 

Thank you and best regards

 

Hans

2 REPLIES 2

Re: Access Manager: Is there a Rule "Has No Status" e.g. "Has Status (None)"

Gears Phenom Gears Phenom
Gears Phenom

Good afternoon, I think that such a rule does not exist.


You can look at the document from the Solution Center, which can help you resolve your issue.

 

https://solutions.industrysoftware.automation.siemens.com/
Document ID: 001-9318286

Re: Access Manager: Is there a Rule "Has No Status" e.g. "Has Status (None)"

Creator
Creator

Thank you for the quick answer.

Exactly the solution I'm searching for :-)

 

Best Regards

Hans