Cancel
Showing results for 
Search instead for 
Did you mean: 

Active Workspace Model Viewer

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Looking into Active workspace, and what the underlying technology that is behind the model that you can view.
Background:

I will be moving some info from one instance of Teamcenter to another.  In this discussion I mentioned for our test, we would move a BOM and its associated JT Models.  Another person said I needed NX models to view in Active Workspace.  Now I have no working knowledge of Active Workspace, so I am looking for some assistance here as to what kind of model the client would be looking at in Active Workspace.  Is it the NX Model? JT?  Some other representation?
Joel

1 REPLY

Re: Active Workspace Model Viewer

Genius
Genius

Lindy,

 

AFAIK, It the models which users will see on the AWS are JT's and i don't think users will be able to view the native files through AWS.

 

Hope this helps !

Cheers.

Teamcenter 10.1.7
TC Visualization 10.1.7
NX:11.02 | NX 9.02 | Catia V5 R2012 | AutoCAD 2018 | In-Context Editor |