Cancel
Showing results for 
Search instead for 
Did you mean: 

Active Workspace define differen number of columns?

Hi,

 

Is it somehow possible to define different number of columns for each section on a stylesheet (XRT) in AWC?

 

I think something has changed. On the stylesheets for the summary in the rich client I was able to define a section and in this section several columns, but this seems not possible for AWC stylesheets.

 

I found a way to do it with HTML panels, but there I had the issue that I was not able to use dynamic compound properties (AWC 3.3).

 

 

In general is there a good manual which gives an overview of all options which are available on stylsheets?