Cancel
Showing results for 
Search instead for 
Did you mean: 

Add DirectModel dataset to Project

Valued Contributor
Valued Contributor

Hello All,

 

Does anyone know if there is a way to include Jt files (DirectModel) when using the "Update_Project_Bom" utility?  Or to make JT files inlcluded in a project without having to select them 1 at time?

 

Thanks in advance!!

 

 

Jake
5 REPLIES

Re: Add DirectModel dataset to Project

Genius
Genius

I think you need mentioned level parameter with value 2 here

 

Level 2 propagation: collect all dataset type objects attached to the revision
items in the BOM structure during the level 1 propagation. Recursively locate
all objects that relate to the dataset type objects through the relation specified
in the TC_project_propagate_from_dataset preference and propagate all
of these level 2 dependencies into the projects.

Re: Add DirectModel dataset to Project

Valued Contributor
Valued Contributor

@Bhojraj,

 

Would a valid value for this preference be "DirectModel"? if you were wanting to blanket the JT files (DirectModel datasets) to add to the project?

 

That is what I had set before, it did not seem to work.

 

Thanks

Jake

Re: Add DirectModel dataset to Project

Genius
Genius

valid value for this -level=2. we cannot specifiy the specific dataset to include here. With value 2 it takes all children exist under ItemRevision.

Re: Add DirectModel dataset to Project

Valued Contributor
Valued Contributor

Hi @Bhojraj,

 

Thank you for your response, though I was referring to the TC preference "TC_project_propagate_from_dataset".  What would be the value for this preference in order to correspond with the level 2 propagation callout when running the "update_project_bom" utility?

 

Thanks

Jake

Re: Add DirectModel dataset to Project

Genius
Genius

Hi,

The valid values for this preference could be relation types. This preference accept multiple values.