cancel
Showing results for 
Search instead for 
Did you mean: 

Adding additional processing to the saved search execution

Valued Contributor
Valued Contributor

Hi Guys,

 

Do you have any idea, if it’s possible to define some kind of user exits (or some kind of handler), in order to add additional processing to the saved search execution. (Additional processing during or after the execution.)

 

Something similar exists in the OOTB “Latest Item Revision...” saved search. (Query Type: Local Query Plus Process)

 

Br,

Csaba

Software Engineer
1 REPLY
Highlighted

Re: Adding additional processing to the saved search execution

Valued Contributor
Valued Contributor

If the query is transformed to a user query, than some custom code could be executed.

For this the libuser_exits.dll needs to be rebiult.

 

See the following:

%TC_ROOT%\sample\extract_objects.bat

- %TC_ROOT%\sample\examples\user_query.c

- %TC_ROOT%\sample\link_user_exits.bat 

- %TC_ROOT%/bin/tc_set_query_where_run -u=<user> -p=<pass> -query=<previously created query name> -run=query

 

Software Engineer