Cancel
Showing results for 
Search instead for 
Did you mean: 

Allow Particular Item creation from NX and disallow the same from Teamcenter

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi, There is a requirement that an particular item type should be created from NX and it should not be allowed to create from Teamcenter. If I apply Display rule, it reflects in TC aswell as NX. If precondition, how can I differentiate whether it is being called from TC/NX?. "Fnd0EnableUsageOfDialog" in CreateInput descriptor is not helping. Using Teamcenter 10.1 and NX 11

1 REPLY

Re: Allow Particular Item creation from NX and disallow the same from Teamcenter

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

What you're looking for may not be possible since the products are working as designed. One practice is to create your Items in TC, configure a BOM, and send to NX to create the design. You would have to break that functionality.


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4