Cancel
Showing results for 
Search instead for 
Did you mean: 

Attach Naming Rules

Pioneer
Pioneer

 Hi experts , 

 

I want to attach multiple naming rules for a single custom item .

And i want to get it as dropdown while creating iteam.

 

Thanks

Girish

4 REPLIES

Re: Attach Naming Rules

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

Are you using the new creation wizard? There you do not get a drop down. The rules are shown at the top of the wizard.

2016-12-29 10_23_09-Tc10_14_Oracle_J2EE_AW24 - VMware Workstation 12 Player (Non-commercial use only.png

 

The screenshot shows one nameing rule with two patterns. If you want to add more nameing rules you have to check the online help for  the different conditions that can be applied.

HTH,

xtof

Re: Attach Naming Rules

Pioneer
Pioneer

Thanks XTOF.

I got it.

Re: Attach Naming Rules

Legend
Legend

If you want to have multiple naming rules that generates an id from a serie it will show you a dropdown next the the New button so you can select which one you want to use.

 

 

2017-01-10_12-02-29-562.png

Highlighted

Re: Attach Naming Rules

Pioneer
Pioneer

Yes jormah.

I got it .

 

 

Thanks.