Cancel
Showing results for 
Search instead for 
Did you mean: 

Attaching an item revision form property on an EC to a workflow

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Hello Everyone!

 

I am working on a TC de-customization project where we are attempting to use OOTB handlers to replace the custom ones here at a customer site. For this specific scenario, I would like to retrieve a form property on the Item Revision Master form and check that the property is filled in (not null). I know I can do this using the EPM-check-object-properties rule handler, however, I am unable to attach the property using the EPM-attach-related-objects action handler for some reason. If anyone knows how to go about this, that would be much appreciated! Also, I can definitely provide additional details!

3 REPLIES 3

Re: Attaching an item revision form property on an EC to a workflow

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

SOLVED

 

So I got it to work! Turns out that the relation specified in the Details tab of the rich client was not the correct relation that should be used (could potenitally be a bug), since I was able to get it to work with the IMAN_master_form relation. 

Re: Attaching an item revision form property on an EC to a workflow

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
That form is for the Item. For the Revision you need IMAN_master_form_rev. Keep going!

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Attaching an item revision form property on an EC to a workflow

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

That was the relation that the was specified within the rich client under the Details tab, however, the workflow did not recognize it and outputted an error. I referenced the Doc Center and was able to find the relation above. Please reference the attachment. Thanks for the reply!