Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Attribute Mapping NX

Creator
Creator

Hello,

 

I'm trying to do mapping between NX and Teamcenter.

 

See bellow my mapping's file (which I imported without issue):

 

2018-06-27_11h54_43.png

But when I launch NX and I chose Part Item I don't see my properties:

 

2018-06-27_11h56_41.png

 

How can I display my properties in that window ?

 

Thank you for help.

 

Regards.

3 REPLIES

Re: Attribute Mapping NX

Creator
Creator

I find where I can see my properties:

2018-06-27_12h25_20.png

 

However, after a test, I figure out that my mapping is not working, for exemple that line:

 

AES_MM_MOD_DESCR_L2_EN : Part Revision. ah38_AES_MM_MOD_DESCR_L2_EN /master=both

 

Is there any syntax error ?

 

Thank you in advance.

Regards,

 

Re: Attribute Mapping NX

Gears Phenom Gears Phenom
Gears Phenom

Good afternoon,
I'm not sure, but check out Part Revision try it without a space: PartRevision

Re: Attribute Mapping NX

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hi @Wassim,

 

Take care, you have a space after Part Revision and I think you need to put ItemRevision like that

 

AES_MM_MOD_DESCR_L2_EN : ItemRevision.ah38_AES_MM_MOD_DESCR_L2_EN /master=both

 

Best regards,