Cancel
Showing results for 
Search instead for 
Did you mean: 

Audit file attach as dataset under ItemRevision

Valued Contributor
Valued Contributor

Hello all,

 

Can anyone tell me who to use Audit Manager to get USER_get_additional_log_info handler which adds all singoff information as a txt dataset and attaches under ItemRevision.

 

Thanks a lot.

 

Regards,

Srinidhi

TC9.1 TC11.2

NX8.5 Nx10

3 REPLIES 3

Re: Audit file attach as dataset under ItemRevision

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

USER_get_additional_log_info is an Audit Manager handler that can be used to specify that workflow events gets stored in the audit log. In the help files, USER_get_additional_log_info is defined like this: "Logs workflow information to Audit logs."

 

It's not capable to creating a text file, or of attaching a text file to an Item Revision.

Arden Bedell | Teamcenter Wonk | Applied CAx, LLC

Re: Audit file attach as dataset under ItemRevision

Valued Contributor
Valued Contributor

Hello Arden,

 

So is there any way to use Audit Manager to create a dataset at the end of the workflow to be attached to ItemRevision. or any Handler which can do that?

 

Regads,

Srinidhi

Re: Audit file attach as dataset under ItemRevision

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

None that I know of without custom programming.

Arden Bedell | Teamcenter Wonk | Applied CAx, LLC