Cancel
Showing results for 
Search instead for 
Did you mean: 

Auto checkout on load - TCIC 8.3.7.5

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi,

 

I'm looking for any preference that enables 'auto-checkout' a dataset when it is loaded into catia using 'Load in Catia' option under CatiaV5 menu

 

At the moment, it is not checking out the dataset and users have to manually checkout after it has been loaded into catia

 

Thanks in advance

Sree Harsha

2 REPLIES 2

Re: Auto checkout on load - TCIC 8.3.7.5

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
You can try these prefs:
TC_Auto_Checkout=ON
TC_checkout_and_export=1

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Highlighted

Re: Auto checkout on load - TCIC 8.3.7.5

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Thanks Randy.

 

TC_auto_checkout is set as 'ON' and tc_checkout_and_export is set to '0'.

 

There has to be another way to get my desired behavior because, we load data into catia from "CATIA V5" menu in structure manager and My Teamcenter. TCIC is responsible for loading data. So, I think there has to be some preference in TCIC that controls this behavior.

 

Unfortunately, I could not find any such preference in TCIC documentation

 

Regards,

Sree Harsha