Cancel
Showing results for 
Search instead for 
Did you mean: 

Auto validation in a Review task

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello everyone,


I would like to have a Review task which is automatically validated.

Indeed, the step before is a task condition I can not get the approver in NX, I need a review task to recover the signoff.

Would you tell me if this is possible and if yes how?

Thank you in advance for your help.

Best regards.

4 REPLIES 4

Re: Auto validation in a Review task

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

I found with a quorum = 0 in the handler EPM-adhoc-signoffs.

 

Regards :) :)

Re: Auto validation in a Review task

Legend
Legend

Why not use the simple EPM Task instead?

---

Thanks and Regards

Yogesh Fegade

Re: Auto validation in a Review task

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello @fegade-sot,

 

What I want to do is be able to retrieve the name of the person who validates this task in NX (with the mapping file) but that in fact this task is validated automatically.

I read it is posible to do a mapping beetween NX and a Review task, but unfortunately with the quorum = 0 it does not consider that the user has validated so he does not recover it in NX.

 

Maybe do you have an idea ?

 

Best regards,

Highlighted

Re: Auto validation in a Review task

Legend
Legend

You may have to write a custom handler or custom run time property.

---

Thanks and Regards

Yogesh Fegade