Cancel
Showing results for 
Search instead for 
Did you mean: 

Autocad integration issue

Experimenter
Experimenter

Dear All,

 

This is Achyut from India .

 

I am trying to integrate AutoCAD Mechanical 2012 with TC 10.1.4.2  .

 

But unfourtantly i am getting one error while loging to TC from Autocad .

 

AUTOCAD error.jpg

 

 

Please suggest me to solve this .

 

Thanks & Regards,

Achyut

3 REPLIES 3

Re: Autocad integration issue

Phenom
Phenom

Hi @Achyut, are you using SOA services API to develope the integration ? If yes, you need to connect using HTTP i.e. 4-Tier client, not a 2-Tier client.

 

(SOA Services is the only way I know to integrate a third party product with Teamcenter)

Re: Autocad integration issue

Experimenter
Experimenter
Hello ,

Thanks a lot for replying .I am not using TCAA_10_1_0 to integrate which we have downloaded from GTAC .
And we have server & client in the same machine .only i am not able to configure server.config to connect to the team center server .

Could you please suggest me on this?

Thanks & Regards,
Achyut

回复: Autocad integration issue

Experimenter
Experimenter

High version of AutoCAD is opened by opening a111.jpgclauncher.exe caused. Because runner.exe detects Aclauncher.exe does not start after the start, so runner that the program has ended, it will delete the relevant files from the directory inside, resulting in can not be opened.
Solution:
Start the registry editor (each client needs to do this configuration)
HEKY_CLASSES_ROOT \ AUTOCAD.DRWAING.XY \ SHELL \ OPEN \ COMMAD
XY: Random value
The value needs to be changed to acad.exe, not aclauncher.exe