Cancel
Showing results for 
Search instead for 
Did you mean: 

Automated export of monolithic JT assembly

Creator
Creator

 Hi,

 

I'm looking for an automated way of exporting an assembly in Teamcenter as monolithic JT-file. The assembly needs to be configured by variant and revision. 

What I'm really looking for is an automated version of TcVis Mockup, Export-> JT (Monotlithic).

 

Do anyone know something like this?

9 REPLIES 9

Re: Automated export of monolithic JT assembly

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
You haven't said which CAD platform you're using to create the JT so I'll assume NX. You can create a dispatcher translator based on the ootb JT translator and use the "monolithic" switch in the configuration file.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Automated export of monolithic JT assembly

Creator
Creator

You are assuming right, we use NX (NX10) and Teamcenter 10 (10.1.2.2). Sry for not stating in first post. We also do create JT files on Dispatcher (ugtopvdirect) when NX models are relased. 

Hence my question, I want to "reuse" the JT files in some way and create a monolithic JT file (or maybe a plmxml (with jt files in a folder)) outside Teamcenter.

 

Yes I'm also aware of this can be done by NX JT Translators (ugtopv) but I think this won't be very performant, the assembly we want to export contains of about 5000 parts. (The size of JT-file we export from TcVis is about 3 Gb )

 

I have also looked into the utility assy_jt_creator which is something like what I want to achieve but this one fails on some of our JT-files (I think the jt toolkit which is used is quite old and our JT-files are new).

 

So I appreciate all suggestions that can export an assembly from TC in JT format in an automated way (something like ug_clone but for JT) (TcVis Export are not possible to automate, as far as I understand :( otherwise this would be the best solution for us)

 

 

Re: Automated export of monolithic JT assembly

Legend
Legend

Hi,

 

try following command for TC-shell

 

C:\PLM\NX9\PVTRANS\run_ugtopv.bat -pim=yes "@DB/TestAssy/A01" -honour_structure -u=xxx -p=xxx -g=xxx -save_outside_teamcenter -force_output_dir=d:\jt -config="C:\PLM\NX9\PVTRANS\tessUG.config"

 

Make sure your tessUG.config has following setting:

structureOption = "MONOLITHIC"

 

Br

Fred

 

Frederik Verscheure
Evolve Consulting bvba
Freelance NX & Teamcenter consultant
frederik@evolve-consulting.be

Re: Automated export of monolithic JT assembly

Creator
Creator

I ended up with running quite a lot of tools to export a complete BOM in JT.

For any one intrested i did the following:

 

Bomwriter (Tc) for extract a plmxml bom

load_fcccache (Tc) to download all of the JT-files

plmxmltojt to convert (Vis) from plmxml to JT

jt2jt (jt utilities) from JT to Monolithic JT

 

Some of my problems are related to corrupt JT-files, but the procedure appove are working at the moment.

 

Highlighted

Re: Automated export of monolithic JT assembly

Legend
Legend

Maybe a little late, but there is an interesting utility that you should checkout. I haven't tried it.

 

 

https://support.industrysoftware.automation.siemens.com/docs/teamcenter/10.1.2/help/index.html#uid:i...

Frederik Verscheure
Evolve Consulting bvba
Freelance NX & Teamcenter consultant
frederik@evolve-consulting.be

Re: Automated export of monolithic JT assembly

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hi, do you have the syntax of the jt2jt tool to create the monolithic?

Thanks.

Re: Automated export of monolithic JT assembly

Siemens Genius Siemens Genius
Siemens Genius

it is included in the Help that comes with the JT utilities. You will need to setup your config file to have the structure option = MONOLITHIC

 

3.1 Purpose

 

The jt2jt utility reprocesses existing JT data. Control of reading and writing the JT files is achieved by specifying a JT Open Toolkit configuration file.

 

3.2 Syntax

 

jt2jt [ –h | -v | –z <config file> ] <infile.jt> <outfile.jt>

 

3.3 Arguments To

Use this option

Display help information.

–h

Print verbose messages.

-v

Specify a JT Open Toolkit configuration file.

–z <config file>

Re: Automated export of monolithic JT assembly

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Thanks a lot Mark.

Did run the tool with the syntax.

 

It helps.

 

Re: Automated export of monolithic JT assembly

Experimenter
Experimenter
Hello,

Is anyone familiar how to create a monolithic JT and exclude the BOM structure in the JT? I would just like the monolithic JT of the assembly alone.