Cancel
Showing results for 
Search instead for 
Did you mean: 

Automatically initiating workflow job on Item

Genius
Genius

Hi

 

Any idea on how we can initiate workflow job automatically on Item-Creation. 

 

 

Regards

Naveen

5 REPLIES

Re: Automatically initiating workflow job on Item

Genius
Genius

Naveen,

I don't think this can be achieved through the configuration !!

 

I am bit curious to know what's the Business case is ? Based on my experience, It doesn't make sense to subject an item / item revision to workflow as soon as it is created. As the data set attached may not be complete.

Only way i see is through the customization. But you have to consider things like:

1) What Item / Item Rev goes thru what workflow process ?
2) Should a workflow task be an Acknowledgement ? whom to assign from the resource pool ?
3) Task duration ? etc etc..

Cheers !

Teamcenter 10.1.3
TC Visualization 10.1.3 (Custom Patch)
NX:8.5 | NX 9.02 | Catia V5 R2012 | AutoCAD 2015 | In-Context Editor |

Re: Automatically initiating workflow job on Item

Genius
Genius

Thanks in advance.

 

The basic requirement is to automatically create a folder directly under Item with a custom folder-name

 

I tried using extension rule "createObjects", but this creates folder with name=itemname (derives name from ITEM)

 

So Im thinking to create 1 step workflow where I can modify above folder name using handler "EPM-Set-property"

 

This is little workaround to create a customfolder(name) under Item Smiley Happy

Re: Automatically initiating workflow job on Item

Legend
Legend

If you don't mind writing customization, then you can use post action method on Item creation/save as events.

---

Thanks and Regards

Yogesh Fegade

Re: Automatically initiating workflow job on Item

Genius
Genius

We want to achieve through configuration only.

 

Is there no way to initiate wf automatically on creation of ITEM?

Re: Automatically initiating workflow job on Item

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Not unless you want to install the Aerospace template. And that will submit a new Item to WF but won't automagically create a Folder or structure of Folders as you want. I only know of codeful solutions for that level of automation.

 

Best,

/Randy


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11.0.1.mp01 | SW 2016 | TcUA 11.2.3
Evaluating:AW 3.2