Cancel
Showing results for 
Search instead for 
Did you mean: 

Automatically obsolete

Experimenter
Experimenter

Hello all,

 

I am wondering if you are able to automatically obsolete an item when a later rev is released through workflow? Can't find anything in the workflow designer guide. We are running TC 9.3.3

 

Thanks,

 

Paul

4 REPLIES

Re: Automatically obsolete

Genius
Genius

AFAIK, there is no out-of-the-box functionality. We had to develop a customization as in our case, The previous item may or may not obsolete. We have different statuses, Service,Obsolete. Etc.

 

BTW, we are using TC 10.1.3 and we are using the customisation.

 

Hope this helps !

Cheers.

Teamcenter 10.1.7
TC Visualization 10.1.7
NX:11.02 | NX 9.02 | Catia V5 R2012 | AutoCAD 2018 | In-Context Editor |

Re: Automatically obsolete

Legend
Legend

You can use this handler: TCX-release-previous-itemrevs 

 

Description:
Sets a status on the current revision's preceding item revisions, dependent on their current status. Subsequently, the specified item revisions can optionally be sent into a workflow.

 

Regards

Naveen

TC9.1

Re: Automatically obsolete

Experimenter
Experimenter

Thanks for that - the TCX-release-previous-itemrevs seems to work fine.

 

Obviously will need to test it a little more but signs are promising.

 

Many thanks,

 

Paul

Re: Automatically obsolete

Legend
Legend

You are welcome Paul.

 

To make things more easier for you, create a new workflow template called "Quick Obsolete...".

 

Use the handler with argument -proc_name="Quick Obsolete".

Assign this new WF template for admin for addressing day to day support issues.

 

Regards

Naveen