Cancel
Showing results for 
Search instead for 
Did you mean: 

BMIDE - Check Latest Released

Valued Contributor
Valued Contributor

Dear Listers,

 

I am trying to change the value of the maxAllowedWorkRevs to 1 so that I cannot create more than 1 working revisons

How ever when I am checking the extension  -- checkLatestReleased I see the buttons on the left are greyed out as in the attached PNG.

I later realised that my Teamcenter 10 (10.1.7.1(20170205.00))  is at Business Modeler IDE (10.1.0) and not patched.

 

Is this the reason for the controls on the right of the extension is disabled.?

How can I patch the BMIDE to 10.1.7.1 manually?

 

Regards

Vilas

2 REPLIES 2

Betreff: BMIDE - Check Latest Released

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

You can't and shouldn't modify the ' checkLatestReleased' extension. It is a foundation object.

Just add this extension as Pre-Condition under the item_copy_rev operation of you Item Revision Business Object. Find item_copy_rev operation in the operation tab.

Michael
Teamcenter UA | NX CAD

Betreff: BMIDE - Check Latest Released

Solution Partner Esteemed Contributor Solution Partner Esteemed Contributor
Solution Partner Esteemed Contributor
Hope this helps...

For MaxAllowedWorkRevsForItemCopyRev to be processed the user has to set the precondition checkLatestReleased on the ITEM_copy_rev operation of the ItemRevision Business Object. Once checkLatestReleased is set and MaxAllowedWorkRevsForItemCopyRev is set to a number >=1, its value will be checked and a warning message will be presented to the user, it the user tries to create more revisions than those set by MaxAllowedWorkRevsForItemCopyRev.

Firstly I created a project in BMIDE and in order of business object=> Item Revision => top tab(Main) sub tab(Business Object Constant). In Business Object constant; there are 3 values to change (MaxAllowedWorkforRevsforItemCopyRev,MaxAllowedWorkforRevsforItemCreate,MaxAllowedWorkforRevsItemCpRevexist) this values default "-1",this means you can create unlimited revisions. But when you change the values to "1",therefore only one working revision on the System. After that you should attach "checkLatestReleased" to Item Revision(Operations tab)=> there are 3 values (ITEM_copy_rev,ITEM_copy_rev_to_existing,ITEM_create_rev). You should add "checkLatestReleased" to them. (I think this way include all revisions)

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4