Cancel
Showing results for 
Search instead for 
Did you mean: 

BMIDE-Update and Database-Update neccessary after Update TC_BIN and TC_DATA

Builder
Builder

Hello,

 

I have update now Teamcenter 10.1.2 to 10.1.6.1. After that I have update TC_DATA-directory manually.

Do I have to update BMIDE and Database separately via TEM with the feature_foundation.xml or is it done with updating TC_BIN?

 

Michael

Michael Eichelberg, CAD-Consultant, Dr. Wallner Engineering Nord GmbH
Production: NX10.0.3 MP16, NX11.0.1 MP4
Development: Batch and VB Testing: NX12
1 REPLY

Re: BMIDE-Update and Database-Update neccessary after Update TC_BIN and TC_DATA

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

There is a "templates" folder under BMIDE and it contains a copy of the foundation template.It uses the templates in this folder when you open BMIDE to work on business objects, etc.

 

If BMIDE was one of the features that were installed with the rest of Teamcenter, it will be updated at the same time as the rest of Teamcenter, and that includes updating the foundation template in the "templates" folder.

 

If BMIDE was a separate install from the rest of Teamcenter you will have to go through the upgrade process again using the copy of TEM in its "install" folder. This upgrade will also upgrade the foundation template in the "templates" folder.

 

In either case, you don't have to manually update the foundation template.

Arden Bedell | Teamcenter Wonk | Applied CAx, LLC