Cancel
Showing results for 
Search instead for 
Did you mean: 

BMIDE deployment error, File not found

Builder
Builder

Hi all

 

I've an error in deployment command of BMIDE. After a while deployment stops with error: "File not found" and no more information.

 

It's obvious that the error happened in step 9 business_model_updater.exe command but not the info isn't enough.

 

The project deploy log file is as follow:

 

LogFileName    : Deploy.log
TimeStamp      : 03-Jul-2018
Options        : Full Update
Deploy Source  : BMIDE
------------------------------------------------------------------------------------------------------------------
------------------------------------------------------------------------------------------------------------------
Deploy Summary
------------------------------------------------------------------------------------------------------------------
*****  BMIDE deployment lock utility results  *****
*****  BMIDE deployment lock utility is successful  *****
Deploy Step 1 of 9: Success
Deploy Step 2 of 9: Success
Deploy Step 3 of 9: Success
Deploy Step 4 of 9: Success
Deploy Step 5 of 9: Success
Deploy Step 6 of 9: Success
Deploy Step 7 of 9: Success
Deploy Step 8 of 9: Success
Deploy Step 9 of 9: ** Failure **
---------------------------------------------------------------------------------------------------------------------
Deploy Step 1 of 9:
---------------------------------------------------------------------------------------------------------------------
Description: Validating template for deployment 
Result: Success
---------------------------------------------------------------------------------------------------------------------
Deploy Step 2 of 9:
---------------------------------------------------------------------------------------------------------------------
Description: Adding entries to the master.xml file
Adding the following entries:
bm2johnbide_template.xml
Result: Success
---------------------------------------------------------------------------------------------------------------------
Deploy Step 3 of 9:
---------------------------------------------------------------------------------------------------------------------
Description: Backup the existing model.xml file to model_backup.xml. 
Consolidate all templates into the <TC_DATA>/model/model.xml file.
Backing up model.xml to model_backup.xml.
The file model.xml is copied to: C:\PROGRA~1\Siemens\tcdata\model\model_backup.xml
Result: Success
---------------------------------------------------------------------------------------------------------------------
Deploy Step 4 of 9:
---------------------------------------------------------------------------------------------------------------------
Description: Creates a backup of model_lang.xml into model_lang_backup.xml.
The file model_lang.xml is copied to: C:\PROGRA~1\Siemens\tcdata\model\lang\model_backup_lang.xml
Result: Success
---------------------------------------------------------------------------------------------------------------------
Deploy Step 5 of 9:
---------------------------------------------------------------------------------------------------------------------
Description: Consolidate templates from master.xml to model.xml. 
The full path to the master file:C:\PROGRA~1\Siemens\tcdata\model
The full path to the file that should be generated: C:\PROGRA~1\Siemens\tcdata\model\model.xml
Result: Success
---------------------------------------------------------------------------------------------------------------------
Deploy Step 6 of 9:
---------------------------------------------------------------------------------------------------------------------
Description: Extract the list of allowable Live Update elements
from the database into the live_update_preference.xml file.
The Process Mode is not Ops Data
Result: Success
---------------------------------------------------------------------------------------------------------------------
Deploy Step 7 of 9:
---------------------------------------------------------------------------------------------------------------------
Description: Loads the new model (deployed from BMIDE) and the old model (previous) 
to compute the elements that were added, deleted, or changed in the BMIDE. 
Verifies that each of these elements are permitted to be updated by verifying against 
the Live Update Elements List from the database. Writes the added, deleted, changed elements to a delta.xml file.
Loading the Backup File...
Loading the Consolidated File...
Comparing the two Files...
Creating the Delta file...
Result: Success
---------------------------------------------------------------------------------------------------------------------
Deploy Step 8 of 9:
---------------------------------------------------------------------------------------------------------------------
Description: Compares model_lang.xml and model_lang_backup.xml and generates delta_lang.xml.
Comparing the two Localization Files...
Creating the Localization Delta file...
Result: Success
Uploading the project backup files to Database...
	 Processing File:bm2johnbide_project_tc11000.4.0.zip
Result: Success
Uploading the project icon files to Database...
Result: Completed uploading the project icon files 
---------------------------------------------------------------------------------------------------------------------
Deploy Step 9 of 9:
---------------------------------------------------------------------------------------------------------------------
Description: Process the delta.xml file committing each data model element to the database.
Executing: business_model_updater.
Result: Failure

Could anyone help me?

Thanks for your attention

 

14 REPLIES

Re: BMIDE deployment error, File not found

Phenom
Phenom

Good afternoon, business_model_updater.exe it should also generate a log, you need to look at it for errors or put it here

Re: BMIDE deployment error, File not found

Builder
Builder

@ArthurRM wrote:

Good afternoon, business_model_updater.exe it should also generate a log, you need to look at it for errors or put it here


Thanks @ArthurRM

The business_model_updater**.log file was empty, but I found the bmide_manage_templates**.syslog with the following error:

ERROR - 515035: The input string is too long.
ERROR - 515035: The input string is too long. - ERROR: 515035 ERROR MSG: The input string is too long.. - Teamcenter.main at D:\workdir\tc1140x_win64\src\core\main\bmide_manage_templates_itk_main.cxx(435)

Actually I think its due to a failed bmide template installation (SWIM) and I've no backup before that. Is there any way to make it correct?

Any solution?

 

Thanks

 

Re: BMIDE deployment error, File not found

Phenom
Phenom

I have a question, do you install the SWIM Template using BMIDE? This is an OOTB template and is usually installed using the environment manager (tem.bat). Do you install the template bm2johnbide_project_tc11000.4.0.zip? It's just not like the SWIM Template.

When you install the templates, judging by your log, you have backed up the xml of your data model:

Backing up model.xml to model_backup.xml.
The file model.xml is copied to: C:\PROGRA ~ 1\Siemens\tcdata\model\model_backup.xml

Re: BMIDE deployment error, File not found

Builder
Builder

Thanks @ArthurRM

 


@ArthurRM wrote:

I have a question, do you install the SWIM Template using BMIDE? This is an OOTB template and is usually installed using the environment manager (tem.bat).


No, I used TEM to install it, but as I mentioned before error 515035 happened during the installation process and unfortunately I had no backup before that.

 


@ArthurRM wrote:

Do you install the template bm2johnbide_project_tc11000.4.0.zip? It's just not like the SWIM Template.


Yes, It's my test template which I applied it after SWIM. I just wanted to test if BMIDE and tcdata work correctly but no chance.

 

Would you think if its possible to manipulate model.xml to remove failed SWIM template installation?

Actually I've not enough information about TCDATA content and its affect on TC process and which files are changed after any template installation (Like SWIM).

 

Thanks

Re: BMIDE deployment error, File not found

Phenom
Phenom

I have not encountered this error, here's what you can try to do:

1) Try to remove SWIM from tem.bat (select modify component, and try unselect SWIM)

2) You can return to the previous configuration, as described by RandyEllsworth in this thread:

https://community.plm.automation.siemens.com/t5/Teamcenter-Administrators-Forum/tem-bat-stuck-in-rec...

And try reinstall SWIM template. Before reinstalling, save a copy of the current configuration.xml so that you can return to the current state

3) Try remove bmide template from teamcenter, but I never tried to delete it

https://community.plm.automation.siemens.com/t5/Teamcenter-Administrators-Forum/remove-bmide-templat...

4) Contact to GTAC

Re: BMIDE deployment error, File not found

Solution Partner Genius Solution Partner Genius
Solution Partner Genius
I tired to replicate this bug and I can't figure out when it exactly occurs. I have 2 environments OOTB TCRS + AWC (11.4.7 + 3.2.3) both with the same issue. The installation wet fine but when I run bmide_manage_templates tool to list installed templates I receive 515035 Error message before any attempt to install additional data model.

Re: BMIDE deployment error, File not found

Phenom
Phenom

Hello, try to look * .syslog, which generates bmide_manage_templates for more information about this error

Re: BMIDE deployment error, File not found

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Nothig usefull besides 515035 error information. This is DEBUG version of log.

Re: BMIDE deployment error, File not found

Phenom
Phenom

Look in the solution center document ID: 001-7787351 If it does not help you, I think you need to contact GTAC