Cancel
Showing results for 
Search instead for 
Did you mean: 

BMIDE deployment error TC10

Experimenter
Experimenter
Hi, When I deployed the custom template to TC by BMIDE an error message is encountered as "Internal Error in BMIDE Module". Before deploying above custom template, we have removed one other custom template from TC. We removed all instances from that template and successfully removed custom template, No error shown till end. But when We trying to deploy another custom template got and error, snap is attached with this post. Please help to solve this problem as soon as possible.
2 REPLIES

Re: BMIDE deployment error TC10

Phenom
Phenom

Good afternoon, unfortunately according to your screenshot there is not much to say
it is necessary to lay out the installation log that generated the BMIDE

Re: BMIDE deployment error TC10

Pioneer
Pioneer

Hi,

 

If you see there are two properties in "unprocessed schema changes". Those may be referenced somewhere in db and hence not getting deleted. If you could find those references and remove then it's good otherwise, hide those properties in BMIDE so that those would not be available to end users.

 

Br,

Rupesh