Cancel
Showing results for 
Search instead for 
Did you mean: 

Based on Property PLMXML_IMPORT

Dear Listers,

 

I have executed the following steps:

 

1) Created an Item.( eg. TestV)

2) Applied the Item Revision(TestV/1;1) to the custom workflow to attain a custom status ( PILOT)

3) Revised the Item Revision( TestV/2;1)

4) Checked the properties of the new revision(TestV/2;1) and could see the "based on"  property which is Revision 1.(TestV/1;1)

5) Now In the PLMXML_EXPORT in the default TransferMode Which is ConfiguredDataExportDefault. I have added the property set 

CLASS.ItemRevision:PROPERTY.based_on:DO

6) I could export the Item using the PLMXML_EXPORT.

7) In the export file I can see the based_on property reflecting ItemRevsion 1.

8) Deleted the Item( both Revision 1 and Revision 2) , Delated the reference now there is no instance of the ITem(TestV)

9) Did an PLMXML_IMPORT of TestV.xml. But could not see the value in the based_on property.

 

I tried configuring the Propertyset as Type.ItemRevisionSmiley Tongueroperty.based_onSmiley Very HappyO but still it does not reflect the value upon import.

 

If anyone can provide me some pointers to resovle this.

 

Regards

Vilas

1 REPLY

Re: Based on Property PLMXML_IMPORT

Legend
Legend

I haven't tested, but I often find if something doesnt work using PLMXML i switch to TCXML.  Might be worth a try?

 

Rich

 

Richard Bennett
PLM Consultant
www.ProspectPLM.co.uk