Cancel
Showing results for 
Search instead for 
Did you mean: 

CATIA Load Behavior

Experimenter
Experimenter

Hi Everyone,

We have face a CATIA load problem when more than one CATPart dataset attached to ItemRevision with different relation.

We have 2 catia CATPart dataset under ItemRevision.

 

The CATPart1 is connected to ItemRevision with IMAN_specification Relation.

The CATPart2 is connected to ItemRevision with Custom Relation.

When we try to open ItemRevision in CATIA, some item 

When we try to open ItemRevision in CATIA;

     for some ItemRevisions CATPart1 which is connected with IMAN_specification is opened,

    and  some ItemRevisions CATPart which is connected with Custom Relations is opened.

Is there a setting like CATIA's default opening relation?

What is CATIA's default dataset opening behavior?

 

Thanks

1 REPLY

Re: CATIA Load Behavior

Legend
Legend

Hi,

 

TcIC Data model doesnt support two CATPart under single ItemRevision during load process with OOTB configuation.

 

You have to customize the TcIC Entry point here to decide which Dataset to use duing load process.