Cancel
Showing results for 
Search instead for 
Did you mean: 

Can not save modified documents in Solidworks Integration 10.1

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi guys,

 

I create d SLDPRT on Swim 10.1 in Solidworks 2014.

I save it, I get the JT file to be saved into Teamcenter.

Then I close Teamcenter.

 

When I open the item again in Solidworks via Swim, I can open it, modify it.

However, when I click save, I get an error.

qwe.jpg

 

Also, as you can see, I don't have a save checkbox where I can pick the documents to be saved.

Even the SWIM knows it is modified, I don't get an option to save it.

 

Can you help?

2 REPLIES

Re: Can not save modified documents in Solidworks Integration 10.1

Siemens Phenom Siemens Phenom
Siemens Phenom
That screenshot indicates (to me) that the part is not checked out. You need to have it checked out in order to save it into Teamcenter. I have to assume that when you checked it in you used the option for check-in and keep reference. All you have to do is right click on the object in the SWIM toolbar within Solidworks and pick "Check out".

Larry Carpenter, P.E.
CAxPLM Architect @ Siemens Molecular Imaging
Past Board Member @ PLM World, Inc,

Re: Can not save modified documents in Solidworks Integration 10.1

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Thank you Larry.

I thought I had NX Smiley Happy

Cem