Cancel
Showing results for 
Search instead for 
Did you mean: 

Can startup NX from teamcenter with infodba. but can not start NX with other user

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi, I Can startup NX from teamcenter with infodba. but can not start NX with other user. 

I do not know what happened. Our teamcenter is 10, NX is 10. this happened in 2 tier structure.

In 4 tier structure without this problem.

8 REPLIES

Re: Can startup NX from teamcenter with infodba. but can not start NX with other user

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Clear cache first.
Any errors messages?

Re: Can startup NX from teamcenter with infodba. but can not start NX with other user

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

I tried to clear the cache. the problem still exist.

There is a Router window, say Routing to application...

no NX startup.

 

I do not how to check other errors message.

 

I tried to check the processes in Task Manager.

When start NX from teamcenter.

There is a NX process appear

after a few second. the NX process disappear.

only NX Component process in there

 

Re: Can startup NX from teamcenter with infodba. but can not start NX with other user

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Does this forum post help?
https://community.plm.automation.siemens.com/t5/Teamcenter-Administrators-Forum/ERROR-Failed-to-star...

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Can startup NX from teamcenter with infodba. but can not start NX with other user

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

I tried: %UGII_BASE_DIR%\UGII\ugs_router -ugm

the result is the same

Re: Can startup NX from teamcenter with infodba. but can not start NX with other user

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Then go on to the next step and try the MIME type debugging.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Can startup NX from teamcenter with infodba. but can not start NX with other user

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

I run:

runner -mime=application/ugmportal

 

the following message appear in a new window:

Missing n-tier parameter
Press any key to continue . . .

Re: Can startup NX from teamcenter with infodba. but can not start NX with other user

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
That means your mime type is setup correctly. It would be bad if you didn't get the popup.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Can startup NX from teamcenter with infodba. but can not start NX with other user

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Sometimes is quicker to reinstall integration insted fighting with bunch of local properties Smiley Wink