Cancel
Showing results for 
Search instead for 
Did you mean: 

Can't Integration Creo to Teamcenter

Genius
Genius

Hello All

 

I install Teamcenter Integration for Creo 11.4 for 2-tier

Creo is 3.0 MP140

I installed step by step with Installation guide

When I open Creo

I shows me wrong infomation

擷取.PNG

 

I follow application launch issues to find error

But I check all of list,I still don't know where the problem is

Where I need to check?

 

Thanks

Teamcenter 11.2.3,Active Workspace 3.2


Solid Edge ST10
5 REPLIES

Re: Can't Integration Creo to Teamcenter

Genius
Genius

did you check Creo 3.0 compatibility with TC 11.4?

Re: Can't Integration Creo to Teamcenter

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Creo 3 and 4 are supported for Tc11.2.3 (and Tc11.3). The integration is 11.4. Unfortunately, the error is generic and can be many problems. I had this issue until I went back and installed the J-Link API. Once, that was done then the integration started correctly.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11.0.1.mp01 | SW 2016 | TcUA 11.2.3
Evaluating:AW 3.2

Re: Can't Integration Creo to Teamcenter

Genius
Genius
Hello Venny

YES,I check it!

Teamcenter software versions
 Teamcenter 10.1.5.1 and later MPs and patches
 Teamcenter 11.2.1 and later MPs and patches

PTC software versions
 Creo Parametric 2.0 date code M150 or later. Supported Teamcenter versions require JRE 1.7 Update 45
or later

64-bit Creo installations require a 64-bit JRE.
 Creo Parametric 3.0 date code M120 or later. Supported Teamcenter versions require JRE 1.7 Update 45
Teamcenter 11.2.3,Active Workspace 3.2


Solid Edge ST10

Re: Can't Integration Creo to Teamcenter

Genius
Genius
Hello RandyEllsworth

How to install it?
Have any resource?
Teamcenter 11.2.3,Active Workspace 3.2


Solid Edge ST10

Re: Can't Integration Creo to Teamcenter

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Launch the Creo installer, modify existing, Customize...
Select "Creo Parametric", "API Toolkits" > Check "Creo Object TOOLKIT Java and Jlink".

JLinkAPI.png


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11.0.1.mp01 | SW 2016 | TcUA 11.2.3
Evaluating:AW 3.2