Cancel
Showing results for 
Search instead for 
Did you mean: 

Can't install Teamcenter Extensions for Microsoft Office

Genius
Genius

Hello all

 

I can't install  Teamcenter Extensions for Microsoft Office

It shows that I have already install.

How can I deal with it?

I am use office 2016 and TC11.4

03_x_03_16-29-32.png

 

Thank you.

Best Regards
David
Teamcenter 11.4,Active Workspace 3.4
Solid Edge ST10
5 REPLIES

Re: Can't install Teamcenter Extensions for Microsoft Office

Phenom
Phenom

Did you have installed earlier version of Teamcenter Extension for MS Office in the system? Or do you install on a "clean" system?

Re: Can't install Teamcenter Extensions for Microsoft Office

Genius
Genius
Hello Arthur3

Yes,I had installed office 2013 before and I uninstalled it.
Than, Installed office 2016.
It is not "clean" system. It is my work laptop.
Best Regards
David
Teamcenter 11.4,Active Workspace 3.4
Solid Edge ST10

Re: Can't install Teamcenter Extensions for Microsoft Office

Phenom
Phenom

Try uninstall Office 2013 or Office 2016 with the easy fix tool from Microsoft:

 

https://support.office.com/en-us/article/uninstall-office-from-a-pc-9dd49b83-264a-477a-8fcc-2fdf5dbf...

 

Check that in Control Panel -> Programs and Features there is no Teamcenter Extensions for Microsoft Office, if it is there delete it.

Re: Can't install Teamcenter Extensions for Microsoft Office

Genius
Genius

Hello Arthur3

Sorry, I am late for respond this.
I check Programs and Features,I have a program call teamcenter application for office.
So I delete it.
And I reinstall office and Teamcenter Extensions.
The problem solved.
I can install it and use it.
Thanks a lot.

Best Regards
David
Teamcenter 11.4,Active Workspace 3.4
Solid Edge ST10

Re: Can't install Teamcenter Extensions for Microsoft Office

Valued Contributor
Valued Contributor

Hi

 

I had the same problem.

Deinstalled 'Teamcenter application for office' from Windows Programs and Features

Reinstalled Office Extensions via TEM.

After that it worked. (Didn't have to reinstall office). 

 

Thanks for pointing me in the right direction.