Cancel
Showing results for 
Search instead for 
Did you mean: 

Can't visualize the tool graphic in the NX CAM after connected with MRL

Genius
Genius

Hello folks

 

I just installed the MRL today, but when I try to retrieve the tool from MRL database, the tool graphics is not visualized in NX. How to solve it?

 

Thanks

 

 Capture.JPG

2 REPLIES

Re: Can't visualize the tool graphic in the NX CAM after connected with MRL

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Did you install "Configure Graphics Builder" and the other options when installing MRL?

clip_image010.jpg


Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Can't visualize the tool graphic in the NX CAM after connected with MRL

Siemens Creator Siemens Creator
Siemens Creator

Hi SeanHAI!

 

Please check in Teamcenter Resource Manager:

Can you see the tool component JT files there?

Do you see the UGMaster datasets with part files in the "Attachments" tab?

 

Is NX running in managed mode?

 

So long...

 

   Markus