Cancel
Showing results for 
Search instead for 
Did you mean: 

Can we use Teamcenter licenses on floating basis?

Hello Team,

 

1. I am having 100 Author Licenses, can it be possible to create 200 users and license should get utilised only when users get logged in TC?

or I will be able to create only 100 users as each user is consuming a license.

 

2. what will be the impact if two users are sharing the same credentials for Teamcenter?

8 REPLIES

Re: Can we use Teamcenter licenses on floating basis?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Teamcenter is using named user licensing exclusively, so each active user needs its own license.

There is no way to make it use concurrent licensing.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Can we use Teamcenter licenses on floating basis?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Just to add to the conversation. You can deactivate a user to create a new user. However, you have to deactivate the user then wait until the beginning of the next month before the license is freed and you can create the new user. For this reason, schedule deactivation(s) until the end of the month then you only have to wait a day to create the new user. Deactivating at the beginning of the month you have to wait the entire month before the license is free.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Can we use Teamcenter licenses on floating basis?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Oh, to answer the rest of your question: the impact of sharing credentials. That violates your license agreement with Siemens and your company can be sued while also loosing support. When you signed the license agreement with Siemens you stated that you would comply with named user.

Randy Ellsworth, Teamcenter Architect, Applied CAx, LLC
NX 11 | SW 2016 | Creo 4 | TcUA 11.4
Evaluating: AW 3.4

Re: Can we use Teamcenter licenses on floating basis?

Legend
Legend

yes, number of active users must be equal number of licenses.

 

named licensing politic - buy more licenses, pay more money.

Business, nothing personal(c)

 

Re: Can we use Teamcenter licenses on floating basis?

Legend
Legend

@RandyEllsworth wrote:
, schedule deactivation(s) until the end of the month then you only have to wait a day to create the new user. Deactivating at the beginning of the month you have to wait the entire month before the license is free.

it's  a some madness.. since TC10 users become slaves of license tracking

Re: Can we use Teamcenter licenses on floating basis?

Hello All,

1. This is really something very much new to me, Can't we use
active/inactive status of the user without even bothering about the start
of the month as Randy mentioned in his comment?

2. I understand I can keep only 100 active users if I have 100 licenses.

3. Can I have 200 users for 100 license which will have 100 inactive and
100 active user status at a time?

4. can i write a script which will switch the status from active to
inactive and vice versa?

5. It will be beneficial for the employees working in shifts even those are
using same systems for work.

Re: Can we use Teamcenter licenses on floating basis?

Legend
Legend

@GaneshDasmale wrote:
Hello All,

1. This is really something very much new to me, Can't we use
active/inactive status of the user without even bothering about the start
of the month as Randy mentioned in his comment?

2. I understand I can keep only 100 active users if I have 100 licenses.

3. Can I have 200 users for 100 license which will have 100 inactive and
100 active user status at a time?

4. can i write a script which will switch the status from active to
inactive and vice versa?

5. It will be beneficial for the employees working in shifts even those are
using same systems for work.

3. - Yes

Re: Can we use Teamcenter licenses on floating basis?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

For the workspace where multiple users work in a shift system, a workspace user is used.

For example the machine operators of one machine share the machine account created in Teamcenter, since they work in a shift and there is always only one user out of the three using the license.

Instead of having users MachineOperator1, MachineOperator2 and MachineOperator3, you have user Machine4715, for example.

This is still not violating the license agreement and you keep yourself from creating hundreds of users.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.1, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide