Cancel
Showing results for 
Search instead for 
Did you mean: 

Cannont delete DXF from Teamcenter

Gears Phenom Gears Phenom
Gears Phenom

User needs to replace a DXF file in Teamcenter, so they want to delete the old one.  The item, and item revision are not checked out by anyone, but TC will not let the DXF be deleted.  User was able to drag-n-drop the new DXF into the item revision, but now there are two DXF files, with the same name, which Murphy's Law will have the wrong one used.

 

Tried logging in as DBA, but still cannot delete the DXF.

 

Thoughts?

 

TC 10.1.0

-Dave
NX 11 | Teamcenter 11 | Windows 10