Cancel
Showing results for 
Search instead for 
Did you mean: 

Cannot open NX from Teamcenter

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi guys,

 

I can open managed NX from start_nx_manager.bat file, with my user credentials, no problem.

I can work with that.

But when I open Teamcenter and hit the NX button from Home, or any Item revision or a UGMASTER, The screen is stuck with this. Nothing happens.

Where should I check?

1.png

 

There are 3 clients on the network, 2 is in this situation but the last one can open NX from TEAMCENTER.

 

Cem

4 REPLIES

Re: Cannot open NX from Teamcenter

Pioneer
Pioneer
Is the Feature. NX Integration for Rich Client (or similar) installed?
Check using TEM.
Thomas Zwatz, CADadmin, PÖTTINGER Landtechnik GmbH
Production: NX10.0.3.5 MP11 + TC10.1.7.1
Testing: NX10.0.3.5 MP17, NX11.0.2.7 MP02 + TC10.1.7.1
Development: C#

Re: Cannot open NX from Teamcenter

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Of course, maybe I put it wrong, It used to work before.
But then I went to admin pool from the Internet Explorer and restarted the user's servers. Then it started working again.
I couldn't relate the problem with that but it worked.

Re: Cannot open NX from Teamcenter

Esteemed Contributor
Esteemed Contributor

So you are using a 4-tier environment?

 

You can check the syslogs on the pool manager server!

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.0, FBM, MRL 3.1.4 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 10.1
Development: VB.NET, Tcl/Tk    Testing: NX12.0

How to Get the Most from Your Signature in the Community

Re: Cannot open NX from Teamcenter

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

I checked them and there were no errors.

 

As I said, restarting the warm servers did the trick.