Cancel
Showing results for 
Search instead for 
Did you mean: 

Case of the combination of precise and imprecise

Valued Contributor
Valued Contributor

Hi, I have one question.

Recently I learnt the precise/imprecise and revision rule.

 

The questions is: 

Is there any case where the structure is configure by the both of precise and imprecise? If there is, could you tell me the business scenario of it ?

For example: there is one structure (one BOM structure )which has 20 level.

The items of the structure from 0 level to 10 level is configure by precise , but the items of the structure from 11 level to 20 level  are configured as imprecise.  

2 REPLIES 2

Re: Case of the combination of precise and imprecise

Valued Contributor
Valued Contributor

Hello Gimec,

 

This is my understanding for your query. Precise & imprecise structures are completely based on specific industry practice. You can configure your structures in BOM as below . For EG

 

Parent Assm

  - Sub Assm 1 ( Precise)

     - Child 1/A

     - Child 2/A

 - Sub Assm 2 ( Imprecise)

   - Child 3/B

   - Child 3/B

 

Again, some of the organisation may prefer working with Imprecise (Sub assembly) structure prior to release. Once the entire components under the parent ( Root component) are ready to release, they may define the same structure as static ( Precise).

 

More Details/ Understanding : http://plmdojo.com/datamodel/precise-imprecise-bom/#.WO3ytph97cs

  

 

Swapnil Gawas
Testing, Teamcenter 11.2.x | Active Workspace 3.x

Re: Case of the combination of precise and imprecise

Valued Contributor
Valued Contributor

Thank you so much. Ok, I can understand it.