Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Catia TCIC Savemanager Standard Itemtype

Pioneer
Pioneer

Hi Everbody.

At the moment i working ont the Mapping from Catia to Teamcenter.

The most Stuff like Catia Partnumber to Teamcenter Item ID is working.

But i how can i change the Itemtype? At the moment the standard is just "Item".

When i am importing some Assemblys i have to change it manually to the Customer Itemtyp.

I changed the pref "CATIA_savemanager_map_ir_object_type" to different Values, but nothing is working.

Has somebody an Idea?

 

 

3 REPLIES 3

Re: Catia TCIC Savemanager Standard Itemtype

Legend
Legend

Hi,

 

The best way here is define the Item Type with which you want to save Assembly/part from CATIA using preferences below

CATPART_item_type

CATPRODUCT_item_type

 

define real name of Item type as value here.

Re: Catia TCIC Savemanager Standard Itemtype

Pioneer
Pioneer
Yes, it works.
Thanks for the quick Help

Re: Catia TCIC Savemanager Standard Itemtype

Legend
Legend

Great.. 

 

The preference "CATIA_savemanager_map_ir_object_type" should also work here required that you map it to CATIA property who value should be display name of Item.