Cancel
Showing results for 
Search instead for 
Did you mean: 

Change Status Icon

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello Experts,

 

I have a customer that does not have BMIDE but would like to change a status icon. As the released and obsolete status' have the same icons. Naturally this is causing some confusion.

 

Is it possible to change an icon without BMIDE? If so how would I do so.

 

Many thanks

1 REPLY

Re: Change Status Icon

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

In the directory:

D:\Siemens\TC101\TC101_Root\portal\plugins\configuration_10000.1.0

I placed a file called customer.properties

 

The file contains information defined as:

release_status_list.Obsolete.ICON=images/red_circle.png

 

The picture is 16x16 pixels and a .png file

 

Then I created an images folder in the same configuration_10000.1.0 directoy and placed the red_circle.png

 

Exit out of teamcenter and stop the services. Then run the genreg.xml file